Life.augmented

STM8 Discovery

Modify settings and columns
Evaluation Boards for STM8 Product Family
Share Discussion
  
View: 
Post
Edited: 4/14/2012 11:45 AM
stevens.mark
  Posts : 11
STM8S Discovery and CCO
I am new at this so please be gentle with me :)  I am struggling to get the CCO pin to output the current clock frequency and I'm struggling.  I have checked out the examples in the STM8S library (version 2.1), in particular the CLK_MaxSpeed example and I seem to be getting no where.

For the hardware I am just using the Discovery board and I have hooked a scope to CN4, pin 4 which I believe is the CCO pin.

For the software I have distilled the following from various examples:

#include "stm8s.h"
#include "stm8s_gpio.h"
#include "stm8s_clk.h"
 
int main( void )
{
    //
    //  Initialise the clock
    //
    CLK_DeInit();
    CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);    //  CPU Prescaler = 1.
    CLK_SYSCLKConfig(CLK_PRESCALER_HSIDIV1);    //  Prescaler = 1.
    CLK_CCOConfig(CLK_OUTPUT_CPU);              //  Output clock on CCO pin.
    CLK_ClockSwitchConfig(CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSE, DISABLE, CLK_CURRENTCLOCKSTATE_DISABLE);
    //
    //  Initialise GPIOs
    //
    GPIO_DeInit(GPIOC);
    GPIO_Init(GPIOC, GPIO_PIN_2, GPIO_MODE_OUT_PP_LOW_FAST);
    GPIO_WriteHigh(GPIOC, GPIO_PIN_2);
    //
    //  Config done.
    //
    while (1)
    {
        GPIO_WriteReverse(GPIOC, GPIO_PIN_2);
    }
}

The while loop is just me trying to get some other form of output to prove the program is actually running.  I am not seeing any meaningful output on the scope for either CCO or the GPIO.

FYI - I am using the IAR environment.

Any help would be appreciated,
Mark



Tags: STM8S Discovery Clock CCO
Share Post
Posted: 4/14/2012 12:25 PM
stevens.mark
  Posts : 11
Problem solved - seems to have been a deployment problem.  Full reboot seems to have fixed it.

Regards,
Mark
Share Post

Browse Private Forums

NOTE: these forums are exclusive for users of this Extranet!)