Life.augmented

APWorkbench

Modify settings and columns

Audio Processor Workbench software development suite

This forum is dealing with ST APWorkbench software. Please browse existing posts before you create a new discussion. Note: Contents of this forum is public, you should not post any confidential information here. More product information, tools and resources can be found on ST website: APWorkbench
  
View: 
APWorkbench v2.1.0 is onlineUse SHIFT+ENTER to open the menu (new window).
veneri.marco011/12/2014 9:54 AMveneri.marco
231
Directional Sound capturing with STA321MPLUse SHIFT+ENTER to open the menu (new window).
Jon05/14/2015 11:54 PMJon
131
Impossible to record/capture from the MEMS microphonesUse SHIFT+ENTER to open the menu (new window).
erenfeld.david34/27/2015 1:41 PMerenfeld.david
158
Audio Comparing and switching Use SHIFT+ENTER to open the menu (new window).
demir.alkan04/21/2015 5:23 PMdemir.alkan
142
Why can not open speaker tune function of APworkbenchUse SHIFT+ENTER to open the menu (new window).
wan_jung.lin812/11/2014 9:36 PMschaub.alfred
477
Correcting Phase of STA311b System with speaker response?Use SHIFT+ENTER to open the menu (new window).
waechter.bernhard612/10/2014 4:38 AMzhao.yun tao
176
STSpeakerTune for automatic loudspeaker compensationUse SHIFT+ENTER to open the menu (new window).
veneri.marco011/25/2014 12:16 PMveneri.marco
154
APWLink using FT2232HL FTDI ChipUse SHIFT+ENTER to open the menu (new window).
waechter.bernhard211/24/2014 12:44 PMwaechter.bernhard
157
Recording a mono track from 4 MEMS mics array (STEVAL-MKI129V3)Use SHIFT+ENTER to open the menu (new window).
baggio.michele311/12/2014 12:45 PMveneri.marco
223
MKI138V1 (STAudioHub) not communicating with APWorkbenchUse SHIFT+ENTER to open the menu (new window).
lundberg.robin37/21/2014 4:54 PMveneri.marco
217
I've installed the APWorkbench suite but I'm getting the following message when launching the application: "APWorkbench I/O warning: No FTDI driver found, APWLink communication will be disabled…..". Can you please provide more explanation about?Use SHIFT+ENTER to open the menu (new window).
naue_b57/18/2014 3:42 PMveneri.marco
356
More than stereo recordingUse SHIFT+ENTER to open the menu (new window).
shaw.david27/18/2014 3:03 PMveneri.marco
209
What is the STSmartVoice Demo Kit?Use SHIFT+ENTER to open the menu (new window).
naue_b37/18/2014 2:57 PMveneri.marco
298
Choose output channelUse SHIFT+ENTER to open the menu (new window).
hernandez.miguel14/10/2014 12:31 PMveneri.marco
207
STDP4020 Firmware Version DetectUse SHIFT+ENTER to open the menu (new window).
liu.yao.00114/4/2014 9:33 AMveneri.marco
226
How to set a user defined frequency crossover on STA339?Use SHIFT+ENTER to open the menu (new window).
roussel.denys13/23/2014 6:45 AMroussel.denys
245
I’m using the APWorkbench tool to configure a specific Sound Terminal amplifier and tune its processing features. Is it possible to log all the I2C input/output operations performed by the tool during a device configuration?Use SHIFT+ENTER to open the menu (new window).
naue_b11/27/2014 1:59 PMveneri.marco
216
I’ve already an older APWorkbench release on my PC. Should I remove it before installing a newer version?Use SHIFT+ENTER to open the menu (new window).
naue_b11/27/2014 1:50 PMveneri.marco
219
STA350BW: 2ch downmix to 1ch (Mono) with OCFG "00"Use SHIFT+ENTER to open the menu (new window).
breu.florian.00111/22/2014 3:08 AMzhao.yun tao
401
The launch wizard panel of the APWorkbench tool is referring to an APWLink interface, can you please tell more about?Use SHIFT+ENTER to open the menu (new window).
naue_b11/15/2014 5:26 PMveneri.marco
227
What is the APWorkbench simulation mode and when should I use it?Use SHIFT+ENTER to open the menu (new window).
naue_b11/9/2014 11:20 AMveneri.marco
234
Where can I get updated FTDI drivers and which OS are currently supported?Use SHIFT+ENTER to open the menu (new window).
naue_b11/7/2014 4:09 PMveneri.marco
257
Is there any help on the scripting commands supported by the APWorkbench tool?Use SHIFT+ENTER to open the menu (new window).
naue_b112/17/2013 2:45 PMveneri.marco
287
Does the APWorkbench tool supports any scripting language?Use SHIFT+ENTER to open the menu (new window).
naue_b111/12/2013 3:28 PMveneri.marco
287
During the APWorkbench setup process FTDI drivers are optionally installed. Can you explain what it is for and if I should install it?Use SHIFT+ENTER to open the menu (new window).
naue_b111/12/2013 3:13 PMveneri.marco
331
Which OS is currently supported by the APWorkbench suite?Use SHIFT+ENTER to open the menu (new window).
naue_b111/12/2013 2:57 PMveneri.marco
262
Configuration, set-up or help files for APWorkbench with MEMSUse SHIFT+ENTER to open the menu (new window).
moore.jonathan110/1/2013 9:23 AMveneri.marco
305

Most Active users

Statistics

Most Viewed Discussions